Part Number: LM5156H-Q1
Dear team,
1. In below layout recommendation, we suggest separate PGND and AGND, and PGND and AGND should be connected together at the exposed pad. Do these two pins require additional single point connections?
2. In our datasheet, it describes "Do not connect input and output capacitor grounds underneath the device". It means we need to separate PGND and AGND, and connect input and output capacitor grounds to PGND directly, and then PGND make the single connections with AGND at EP, right?
3. If we don't separate PGND and AGND. What are the potential risks? Are there any cases to share?
4. The customer has concerns for the separation GND. In the power side, there will be high frequency voltage and current, which may result in voltage difference between the two GNDs. Is there such a risk? If so, how does our device solve this?

Thanks & Best Regards,
Sherry