Hello,
we tried to use the TPS65279V with input voltage of 5V to get 3.3V@1.4A out of Port 1 and 1.8V@0.2A out of Port 2.
We are not using the I2C interface but external resistor dividers.
Unfortunately on our prototype only 1.8V at port 2 works but port 1 stays at 0V.
We measure the following voltages on the enable pins and soft start pins:
- EN1, EN2: 1.5V
- SS2: 2V
- SS1: 0V
We are wondering about the 0V at SS1. Could this be an issue or is it simple not possible to get 3.3V with 5V input?
Here is a copy of our schematic.
Best regards
Janis