Part Number: BQ77905
Other Parts Discussed in Thread: BQ76930,
Provide case details or comments:
We have a battery management system that incorporates a BQ76930 under processor control and a pair of BQ7790508 in parallel with the battery cells and BQ76930. Due to a battery manufacturing implementation we have found that cell balancing in the BQ76930 causes the BQ7790508's to detect erroneous over voltage conditions.
Unfortunately the batteries can not be rebuilt at this time. There are several firmware workarounds that might alleviate this issue. One of which is to limit balancing time in a way that the BQ7790508 fault detection does not count up to the 5 samples as described in the datasheet, and has the opportunity to count down with balancing turned off.
In order to validate that I need to know the approximate sample time implemented on the BQ7790508. I can't find that information in the datasheet. This diagram does describe the fault detection method.

And I did find this image in an application note that seems to indicate the approximate sample time as ~100mS.

Can you please provide some insight into the sample time implemented in the BQ7790508, i.e. how long it takes to measure 5 consecutive samples and trigger the over-voltage fault?