This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90320U: dual bank configuration

Part Number: UCD90320U
Other Parts Discussed in Thread: UCD90320,

Hi,

We know UCD90320 with dual-bank configuration feature, I Does UCD90320U include dual-bank configurations as well? 

Regards,

Mark

  • Hi

    Yes, UCD90320U is the same as UCD90320.

    Regards

    Yihe

  • Hi Yi He,

    1. If there is image crash problem happening on UCD and there is only one image in the UCD. Can others, like BMC, get information to  know there is image crash then to update image?
    2. For dual bank feature, does that mean it can store two same images in UCD?
    3. From datasheet, Black Box Fault Log to Save Status of All Rails and I/O Pins at the First Fault. Does that means it can instant information of all rail and I/O status, including the voltage value reading, EN/PWRGD signals’ High/low information when fault/error happen?

    Regards,

    Mark

  • Hi

    1. Host will know and decide what to do next

    2. no, it only stores one. the dual bank is only for the fail-safe case where customers want to updates

    3. black box does not include the EN/PGRD signal.

    Regards

    Yihe