Other Parts Discussed in Thread: UCC28730, PMP22557, , TPS40210, TPS40210-Q1
Dear TI e2e Team,
We got the reference design from evaluation board (PMP22557) with part number of UCC28730. In that design given input voltage range is 60V to 120V and output 12V/0.4A. So as per our requirement is it possible to increase the output current by tuning any inductor or resistor values. If possible please let us know and mentioned our design requirements as below.
- > Input voltage range 9V to 150V
- > Output voltage 12V and 1.5A
- > If possible please provide TINA model of this IC.