Hi Team,
For the jitter application of UCC28740, could your help with the following 2 questions?
1. When applying jitter frequency to improve EMI, comparing with non-jitter status, will the load regulationof the non-feedback circuit drop in the flyback circuit? More importantly, will the voltage of the non-feedback circuit in light load state go much higher?
2, In order to verify the visual effects of the jitter and non-jitter on load regulation rate, is there any additional circuits are recommended to add to disable the jitter function?
Thanks,
Rebecca