Other Parts Discussed in Thread: TPS560430
Hi Team,
Our customer are evaluating LMZM23600V3SILT at the following conditions.
However, it can’t be started if the output voltage remains 1V.
I guess that LMZM23600V3SILT can’t support Startup with Pre-Biased Output.
Is my understanding correct?
<Conditions>
VIN=24V
VOUT=3.3V (1V remains at startup)
And, I understand that TPS560430 can support Startup with Pre-Biased Output.
So, it can be started even if the output voltage remains 1V.
Is my understanding correct?
Regards,
Hide