Hi expert,
Our customer want to use TPS74901.
Their application is below,
VIN: 1.1V
VOUT: 0.9V
IOUT: 0-2A
VBIAS: 5V+/-5%
VOUT RIPPLE: 6mVp-p
Their dropout is 1.1-0.9=0.2V.
But our spec is max 280mV @ 3A.
And I didn't find max spec @2A. Below is just typ value.
So could you help to confirm can customer use in such application?
Thanks
Best Regards
Sean Song