This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: bq34110

Part Number: BQ34110

Hello.

I have some questions about bq34110.

1. Which pin is the voltage measured by the Voltage () register? Is it the voltage measured between the BAT pin and the SRN pin?

2. What is the current value of high rate when measuring CEDV data? Is it the maximum value in the actual machine or the current value of 1C?

3. What is the current value of lowhrate when measuring CEDV data? Is it the minimum value in the actual machine or the current value of 0.1C?

4. Is it okay to think that FitMaxSOC%, FitMinSOC%, and LearnSOC% of "Configuration File" sent at the same time as CEDV data are around the following?

 Should these three be below the knee?

5. Is SOC changing rapidly? At low temperatures, SOC changes rapidly from 24% to 7%.

Thank you.