This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: overvoltage protection for the PACK pin

Part Number: BQ40Z50

hi Team,

the bq40z50 PACK pin has the asb max voltage value at 30V

with the more common design of type C PD supporting 48V from the type C connector as a charging option to the battery pack.

customer wants to check if there is any recommendations from the pack design to protect against the possible higher voltage such as 48V input to the connector of the pack.

Thanks