Other Parts Discussed in Thread: TPS62130, TPS62903
Hi,
Looking at page 14 of the datasheet the peak inductor current is calculated at 3.46A.
Trying to replicate the design in webench, I get a value L Ipp of 2.08A.
Can you advise why there is a difference here?
I don't need that exact design of supply, I was just trying to get a baseline in Webench. What I'm ultimately interested in is how to spec the inductor current wise for the two following output voltages if you can help there?
Vin 5V -> 5.5V
Vout 1 -> 1.5V 3A
Vout 2 -> 1.1V 3A
Many thanks,
G