Other Parts Discussed in Thread: TPS54201
Hi.
I'm using the DRV8210DSG as a static switching H bridge in conjunction with a tps54201 as a bidirectional TEC driver. Since the DRV8210 is on the high side of the current sense resistor, it is subject to up to a 1V transient in case of a short circuit in my load,
In order to protect the PH input, I was going to put in a small diode to clamp the voltage between the input and the GND to one diode drop. So if my control input is high, the pin will have ~3.3 V on it, and all is well. If the control input is low, the diode will conduct when the pin goes below the GND level, which is at a positive ~1V. See the diagram. Does this seem like it will work for this purpose?
Thanks!
John