When the output is short-circuited (CH1), the waveforms of SS pin (CH1) and CS pin (CH2) are as follows, CS pin tops to nearly 2V and then returns to 0V. look at the SS pin from high to low but cannot recover.
Want to know if there is any internal mechanism of the UCC2895 SS pin that causes the SS can't recover?
Note: I can make sure the REF pin still have 5V during the fail status.
BR, Gary