Hi,
My customer used the UCC29002 in parallel with two 1000W power supplies, and there has been a start-up issue.
Because the start-up time of the two sets of power supplies is different, it will cause the OPP condition.
Is there any solution to reduce this problem?
Schematic
Set up
C2, C3 Vcc start-up time
C1, output current
input 100V, 42A full load start-up
input 230V, 42A full load start-up
Thank you very much for your time and consideration.