■Conditions
Input voltage: 48V
Output voltage: 42V
Output current: 2.4A(MAX)
Is CFF required?
The result of the calculation using the formula in the specifications is a large number, over 100pF.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The Fsw is about 2MHz which is too high for 48V to 42V because of Toff-min limitation and thermal issue.
Pls check if 400KHz workable for you
B R
Andy
Andy.
Thank you for your response.
I have an additional question about the heat dissipation design.
My question is based on the RθJA vs Copper Area graph in the specification sheet. (P.44)
Example) 4-layer board
Am I correct in understanding that RθJA will be approximately 19°C/W if the total area of GND from layer 1 to layer 4 is secured to be 40 mm x 40 mm or more?
Or is a GND area of 40㎜×40㎜ required for each layer?
Hi
It's the GND area required for each layer, i.e, the board size is 40mmx40mm
B R
Andy