Hi,
This is in reference to gate driver IC: UCC21750-Q1. I want to clarify for below mentioned points.
The above mentioned gate driver is finalized to drive a SiC MOSFET with rating >1kV and current around 220 A in our application.
- In case of short circuit protection, there are various methods available such as D-SAT, shunt resistor and sense-fet. However, as per my knowledge, to implement sense-fet protection separate I-sense pin apart from kelvin-sense pin is required, right? And if that pin configuration is not available than can we implement current sense-fet by external means?
- I would like to know which is the most appropriate option for short circuit protection with above mentioned specifications of the SiC MOSFET? As, D-SAT is more preferable in IGBT. Besides the RMS current for the current application is around 79 Arms (just for your information).
- I have gone through relevant threads related to UCC21750-Q1 on E2E forum which are relating to D-SAT circuit calculation and how to add extra charge pump in the blanking capacitor as internal is only related to 500uA. Will share some more thoughts in subsequent conversation.
- There are different available options with the family of UCC217xx such as OC pin and DESAT pin for SC protection. Can you provide some information on which is the best option that can be used for SC protection of SiC-MOSFET? and how?
- If we have used bipolar supply for gate drive such as +18/-4V, still implementing miller clamp circuit can be advantageous? If not, than there is AMC in UCC21750-Q1, so should we connect it to the gate pin of should it be grounded?
Thanks, looking forward for answers.