Hi TI Teams,
Is there a complete solution recommended for charging/discharging and protection of two batteries with different capacities in parallel? The battery voltage is 4.2V, and one of the batteries is removable. The capacity of those two battery is 150+100mAh, or 200+150mAh, or some other combination, but none of them will exceed 300mAh.
Thanks,
Kind Regards