This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: About Short circuit protection

Part Number: TPS1663

Hello,

Short circuit protection is described in the electrical characteristics of the data sheet as follows.
(question)
Does 45A indicate the maximum current that flows through the FET during a short circuit?
Or does it mean that it is okay to flow 45A in the event of a short circuit?

Best regards,

  • Hi Kaji,

    During short-circuit, the turn-off response depends on the magnitude of the short-circuit current

    The device has fast-trip threshold set at 2xIOL i.e., 2 times the current limit value. For example, if you set 6A current limit, the fast-trip threshold will be 12A. the short-circuit current around that will takes 3.2us to respond.

    If the short-circuit impedance is very low causing large short-circuit current exceeding ISCP 45A, then the device will turn-off in 1us (typ)

    Best regards,

    Rakesh