If low ESR/high capacity output capacitors are used, is there a limit? We are a bit concerned of the high in-rush current when the charge pump starts. Is 50µF ok?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If low ESR/high capacity output capacitors are used, is there a limit? We are a bit concerned of the high in-rush current when the charge pump starts. Is 50µF ok?
Hello Alexander,
I do not expect issues with 50uF of output capacitance on the LM2766.
The startup time might be longer as the flying capacitor is most probable relatively small compared to the output capacitor, so you should check if the load does not already discharge the cap when it did not reach the voltage level you want to see.
Best regards,
Brigitte