Other Parts Discussed in Thread: GPCCHEM, , BQSTUDIO, BQ34Z100-G1
Hello,
Is anyone available to help with a ChemID match?
Target Battery Pack is 24V comprised of two BB EVP35-12 35Ah Sealed Lead Acid VRLA AGM Standard Type batteries in series.
I can provide the data sheet if needed.
I'm ready to obtain the discharge data needed to search for a ChemID match per Thomas Cosby's Chemistry ID Selection Application Report.
I have a battery analyzer to control the C/10 discharge rate and log the V,I,T data w/ 1s sample rate with CSV file output.
I'm thinking this would be better than using the EVM adapter which doesn't provide for external Temp measurement.
If a log file generated using eqEVSW is preferred it's no problem.
Please advise regarding cell termination voltage, and if for ChemID match purposes, a discharge test of a single 12V battery is preferred over the 24V pack.
Thank you in advance.