(1).Input current limit is settted by REG 0x3FH (Condition RAC:10mohm Sense Resistor) as Chapter 8.3.5.1.
If setting the input current limit center to 4096mA(0b 0001 0000 0000 0000), it has a tolerance by +/- 2% as Electrical Characteristics as below figure.
In this case, please teach the detail of Current Regulation Accuracy +/- 2%? Is it included RAC 10mohm resistor's tolerance and Charger' s tolerance of Amplifer, etc.?
In other words, which is correct Case 1 and Case 2 of below?
Case 1. Input current limit difference is only Current Regulation Accuracy +/- 2%.
Case 2. Input current limit difference is caluculated by (Current Regulation Accuracy +/- 2%) + (RAC Sence Resistor tolerance +/- 0.5%) + (Amplifer tolerance +/- ?? %) +…
If Case 2 is corrent, we must know the above valiation items, and we must calcurate diffrenece from setting 4096mA by using valiation item's tolerance. Please teach it.
(2). Max of Input current limit range is REG 0x3FH(0b 0001 1111 1100 0000)=8128mA/ RAC 10mohm Sense Resistor as Table17 as below figure.
If the input current limit:8192mA has the valiance of Current Regulation Accuracy +2% as above question (1), the actual Input current limit will be 8192mA*1.02 =8356mA?
Or, the actual current limit will be set to 8128mA by satuation even if Current Regulation Accuracy +2%?
(3). Max of Input current limit range is REG 0x3FH(0b 0001 1111 1100 0000)=8128mA/ RAC 10mohm Sense Resistor as Table17.
If current comsumption is 8128mA or more at condition of RAC 10mohm, What is happened about sensing current?
For example, when current is fllowed 9000mA at RAC 10mohm, sensing value is clipped to 8128mA as max?