Other Parts Discussed in Thread: PSEMTHR24EVM-081
Hi All,
please can you review our schematic with TPS7A4001 LDO
Vin = 56V
Vout = 3.3V
Iout = (12mA TPS23881RTQ + 11.3mA ISO1644DW) ~25mA max ; Iout_typ = 15mA
-> is one 10uF 25V 1206 X5R ( effective @ 3.3V -> 9.5uF) enough or should i leave the additional footprint C61 and populate it with 10uF 25V 1206 X5R?
-> on the input is 1uF 100V 1206 X7R (effective @ 56V -> 470nF) is this ok or do i need additional C66 to be populated with 1uF 100V 1206 X7R?
in TIDA-050026 there is similar configuration of LDO and only one 1uF 100V 1206 X7R is used
-> as the 56V comes from a isolated flyback converter do i need some LC or Ferrite bead filter on the input of TPS7A4001?
Best Regards,
David.