Hello,
I ‘m planning to use ideal diode controller (LM74720Q) +mosfet to replace :
- D1 and D2 in the following schematic. The objective is charge the two batteries in (false)“parallel”.
- - D3 and D4 are used to make a redundant power supply. The system will be powered by battery 1 or 2 depending on their state of charge. D3 and D4 are used to do a redundant power supply. The will system will be power by battery 1 or 2 depending of its state of charge.
Is it possible to use LM74720Q to manage this 2 functions?
Will we have problems when the battery voltage drops very quickly?
Best Regards.
Sylvain