Other Parts Discussed in Thread: BQ25713, BQSTUDIO
Hello,
I try to learn on a Fuel Gauge on a fully assembled system.
charger: BQ25713, fuel gauge: BQ27750, Battery: single-cell LiFePO4 3.2V. Until the initial discharge, rest everything is fine, it behaves, how it's described in the manual. When I charge it to full, the full capacity shows more as twice the value it should be. (Nominal capacity is 10000mAh), but it's over 20000mAh when the fully charged flag appears. The time it takes multiplied the current the correct value should be about 10000.BQ27750-DUMP-21-11-11_10000.gg.csv