To margin TPSM8A28 using the UCD, would the capacitor in the margining R-C-R be connected to VSNS-? I don't think the capacitor can be connected directly to GND on the board, right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
To margin TPSM8A28 using the UCD, would the capacitor in the margining R-C-R be connected to VSNS-? I don't think the capacitor can be connected directly to GND on the board, right?
The RC is filtering a pwm signal from the UCD to a DC voltage.
The DC voltage and the other R is injecting a current into the FB pin to offset the output voltage.
The UCD uses a closed loop margining scheme by monitoring the output voltage.
VSNS- should be used for the C of the RCR circuit to use the same reference point as the device.
Another way could be to use the REFIN of SS/REFIN pin.