Other Parts Discussed in Thread: BQ2057,
I am using the BQ2057 to charge a 10Ah battery at 225mA charge current. The MOSFET is not getting too hot, but the BQ2057C is getting to 60C. Since I'm trying to pass this product through UL985, I have a limit of 1/2 Tstorage (or Tj if listed) as my max IC temperature. In this case 62.5C. This leaves me with barely any headroom on temperature.

UB2 is the BQ2057C and I've tried to add as much copper under it as possible.
DB1 is my input diode supplying 5V to the BQ2057. RB6 is my high side current sense resistor and PFB2 is my MOSFET.
Ignore RB1 & PFC3, they are not connected in this configuration.
Here is my schematic.

Here is my simplified schematic. I have a uC that will ground the TS pin to turn off charging, but that is working as normal.
I think I have implemented this very close to the datasheet example.
I can't see why the BQ2057C is getting hot at all. What power is it dissipating? Is there something I can do, besides reducing my charge current to lower the temp of the BQ2057?
Here is what the PCB looks like at steady state with thermal camera.