This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25143: sch. review

Part Number: LM25143

Input voltage is 16-32V, typical 24V;
Output voltage is 12V, Iccmax 40A;
Use single external two-phase output;
Please help to reviewLM25143 Schematic.pdf