Input voltage is 16-32V, typical 24V;
Output voltage is 12V, Iccmax 40A;
Use single external two-phase output;
Please help to reviewLM25143 Schematic.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Input voltage is 16-32V, typical 24V;
Output voltage is 12V, Iccmax 40A;
Use single external two-phase output;
Please help to reviewLM25143 Schematic.pdf
hi team,
one more question: how big frequency of switch is suitable for this big current application?
Hi Eric,
Please complete and send the LM25143 quickstart calculator as it is useful for component selection, loop design, power loss analysis, etc.
Regards,
Tim
Here are some comments on the schematic:
Regards,
Tim