This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H4002-SP: Light Load Efficiency

Part Number: TPS7H4002-SP
Other Parts Discussed in Thread: TPS7H4010-SEP,

Hi,

I asked a similar question about the TPS7H4010-SEP, but i was looking for clearer data on the light load efficiency characteristics of the 4002-SP as well. The graphs below are from the data sheet and its hard to really clarify where efficiencies might land when sub 500 mA. We'd likely have 3.3V input and outputs between 1 and 1.8V with loads varying from tens of mA up to a couple hundred mA.

 

Thanks!

Daniel