This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV752-EVM: TLV752

Part Number: TLV752-EVM
Other Parts Discussed in Thread: TLV752,

Is there any small card (a small daughter board) for TLV752? Much smaller than TLV752-EVM? Even without jumpers for select options. What is the PCB size of TLV752-EVM (Its look very large)?

  • Hi Shai,

    Unfortunately the package that TLV752 comes in (TI's DSQ package) is not a common package so we don't have another EVM that is smaller than this one that can fit this package. The dimensions of the board are 2.75in x 2.25in (69.85mm x 57.15mm), excluding the banana connectors that stick off the board. 

    Regards,

    Nick