Other Parts Discussed in Thread: BQ78350, BQ78350-R1
Hello!
Is it possible using these ICs to make a solution that allows to setup protections and gas gauge for currents greater than 32767 mA and 32767 mAh? For example, now for this, I calibrate the current in half and get a range of up to 65534 mA maximum. But it looks like
this is not the right way, especially about SC protections, even if RSNS bit is used. Simply put - I want to get 200A constant current and greater, what Is correct way to build the sulution on this ICs, if possible?