The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28019A: Input voltage frequency.

Guru 11055 points
Part Number: UCC28019A
Other Parts Discussed in Thread: UCC28180

Hi team,

Does UCC28019A depend on the frequency of the input voltage for operation?
For example, is there a possible problem if the input voltage frequency is very low or very high?

Sincerely.
Kengo.

  • Hi Kengo,

    Thank you for the query.

    Lower end of input frequency close to DC should not be a concern. But increasing the frequency would be possible upto the permissible iTHD% (vs bandwidth of the current loop) defined by the system specifications. For a system designed at 60Hz operating frequency, increasing the input frequency for the same power level the THD is going to increase and power factor will decrease. It should probably support higher input frequency upto 400hz but we do not have test data for this. Alternatively, you check UCC28180 CCM PFC controller.  Please let us know if you require any clarifications.

    Thank you

    Regards,

    Harish