This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65252: USB section not used case sub pins status should be?

Part Number: TPS65252

Hi,

Any one please suggest me, If USB section is not used in my application, then USB pins can be connect to GND or VCC or left as Not connected.

And what happens when connected USB section pins(23,25,26,27 and 28 pins) to GND?

Thanking you,

Sateesh

  • Hi Sateesh,

    Thanks for reaching out! If USB section is not used, please connect USB_EN to GND, other pins can be left floating. If you connect all USB section pins to GND, this USB section will be disabled.

    Hope this will be helpful. Anything unclear, please kindly let us know.

    BRs

    Lucia