Part Number: LM285-1
Dear Sir,
Will you please confirm what is the exact difference between two part numbers.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM285-1
Dear Sir,
Will you please confirm what is the exact difference between two part numbers.
Hello Vicky,
The only differences between the two part numbers are:
Change in reference voltage with current when IZ = I(min) to 20 mA is 12mV @ 25C and 30mV @ -40 to 85C in the LM285LPRE3-1-2 and change in reference voltage with current when IZ = I(min) to 20 mA is 10mV @ 25C and 20mV @ -40 to 85C in the LM285Z-1.2/NOPB.
Reverse Dynamic Impedance when IZ = 100μA, f = 25Hz is is 0.2-0.6 Ohm @ 25C and 1.5 Ohm @ -40 to 85C in the LM285LPRE3-1-2 and Reverse Dynamic Impedance when IZ = 100μA, f = 20Hz is is 1 Ohm @ -40 to 85C in the LM285Z-1.2/NOPB.
Average temperature coefficient when IZ = I(min) to 20 mA is ±20 ppm/C @ -40 to 85C in the LM285LPRE3-1-2 and Average temperature coefficient when IZ = 100 uA is 150 ppm/C @ -40 to 85C in the LM285Z-1.2/NOPB.
NOPB also means that the part does not contain lead.
Best,
Walter