This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC-DC Converter 24-24/10A isolated

Other Parts Discussed in Thread: UCC2897A

Hi,

I want to design DC-DC isolated converter details as below.

Input voltage range :- 17 - 33 VDC

Efficiency :- Above 91%

Output voltage:- 19 to 28 VDC

Output current :- 10A

OCP :- 14A

Protections requirement :- OVP, OCP, OTP, Short Circuit & Under voltage.

Main Switching frequency required min 60Khz and Max 100Khz...

Please suggest reference design or suitable part to start design. Which topology suitable for above specs??

Regards,

Vivek