This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478: Webench simulation

Part Number: LM3478

Hi Team,

We are designing a DC / DC power supply circuit using the LM3478.

The design parameters are as follows.
Vin = 5V
Vout = 40V
Iout = 0 ~ 2mA
Fs = 500 ~ 600kHz (changeable)

The result of the simulation cannot be obtained by changing the parameters a little.
Also, when the circuit is actually manufactured and evaluated, Vout = 40V when Iout = 0mA (load circuit open), but Vout decreases as the load current increases.

Could you give some advice?

Beat Regards,
Tom Liu