This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25306: LED not turn off after removing the adapter (charger with powerpath)

Part Number: BQ25306

Hi,

I want to ask about the STAT pin which doesn't change (indicating LED still turn ON) after adapter 12V is removed. But the load is still active. 

For turning it OFF i disconnected the Load so the LED turns OFF. Is there something wrong with the design ?

I think in normal operation, when the 12V adapter is removed the STAT pin changes (LED turns OFF) for indicating it's not charging although the battery is still loaded. 

Note : 12V comes from USB power delivery. 

Thanks in advance

Regards

Aji