Dear Sirs,
My customer product is Tag related product and they found they can't use TI LDO with the smart enable function.
Without smart enable function will no problem.
As their design, they will use tag at the first power on to conduct and generate a 3.6V/1s period pulse.
With this pulse, they can enable the LDO that for MCU power.
After MCU power on, MCU will control all power and provide LDO EN pin with a stable voltage level.
My question are:
1. Is such a design possible or not? if not, why customer design will ok for non-smart enable function LDO?
2. If yes, why do those smart enable LDO cannot work?
Thanks.