This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: LM7480-Q1 alternative

Part Number: LM7480-Q1
Other Parts Discussed in Thread: LM7480, , LM74700-Q1, TPS2411, LM74721-Q1, LM74720-Q1

Hello ,

I wanted to replace TPS2411 (support max 16.5V) used as oring controller in UCD3138PSFBEVM shown in the below attached screenshot. I have higher voltage application (requirement of 48V) so wanted to use LM7480 ( support max 65V) suggested on e2e forum before. Two options LM74700-Q1 and LM7480-Q1 was suggested and both are out of stock currently and has long lead time. I am in urgent need to implement this for prototyping purpose. Kindly suggest me alternate controller for this which is currently available.

Thanks and Regards,

Priya