Hi,
In the following circuit, can we connect system voltage bus from SRN pin instead of SRP pin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the following circuit, can we connect system voltage bus from SRN pin instead of SRP pin
Hi Akash,
Yes but then the charger cannot distinguish between charge current and system load current. The charge current going to the battery will be reduced by system load current. Also, the charger STAT pin will likely never report charge termination when the battery is fully charged, unless the system load current is less than the termination current.
Regards,
Jeff