Hi, there is a example threshold voltage calculation in the datasheet like below, does this include all the variation? the VITN is min 0.792 to 0.808, so if I consider worst case, do i need to add +/- 8mV to the "839.4mV ~840.6mV" ?
What is worst case VITN+VHYS if VHSY=2% and VITN=0.8V variant is used?