Hi,
I am testing the eval board with 6 capacitors of size 1 F. When the voltage on one of the cells is 4 V, I activate balancing just for that cell. The voltage on that capacitor drops to 2.8 whereas I have set the VCBDONE to 3 V. Do I need to activate OVUV protection separately to use this feature of the GUI? I can see that tUV_CYCLE is 8 ms so I assume worst case scenario, the voltage on the cap should be checked at 16 ms and balancing should be stopped if the voltage is lower than 3 V.