I need to connect two LM5170 EVM to get three level boost converter with an output of 48V/9A. How would be the connection? and how to proceed if it is okat? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to connect two LM5170 EVM to get three level boost converter with an output of 48V/9A. How would be the connection? and how to proceed if it is okat? Thanks
Hi Muhammad,
Yes, it is possible get 3 phase. Please refer to the dataheet 8.4.1.2 Configuration of 2, 3, or 4 Phases in Master-Slave Daisy-Chain Configurations
Best Regards,
Feng Ji