This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28712: UCC28712D

Part Number: UCC28712
Other Parts Discussed in Thread: UCC28C42

Hi Team,

Do you have reference schematic design using UCC28712D  whose

Input is 8V DC - 45V DC 

Output 12V DC / 1.7A DC

I cant able to get the information  from Webench . Kindly share the info to proceeed  further.

Regards

Kumar

  • Hello,

    The UCC28712 has VDD turn-on of around 21 V.  It will not work in this application.

    For the low input range I would recommend a UCC28C42.  If you have questions designing with or using the UCC28C42 so the appropriate applications engineer can help you?

    Regards,