Dear Team,
Could TPS65988 support the PD Type-C charger?
PD 3.1 ERP has 28V/5A and 48V/5A.
May I know Ti PD 3.1 chip status?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
The TPS65988 can only source/sink up to 20V/5A (100W) and is only certified by the USB-IF for PD3.0 (TID#: 1099).
Refer to this forum for information regarding PD 3.1: [FAQ] TPS65987D: New USB Type C PD 3.1 Spec enables Extended Power Range up to 240W (EPR)
Regards,
Raymond Lin