This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

please help recommend alternative part of Diolog/SLG5NT1757VTR

Other Parts Discussed in Thread: TPS22811

please help recommend alternative part of Diolog/SLG5NT1757VTR

  • Hi Josh, 

    Our TPS22811 device would be a good alternative as long as your Input voltage is greater than 2.7V. This device's input voltage range is 2.7V to 16V, with a 10A maximum current from IN to OUT. This device also has quick output discharge, low Ron (6mohm), adjustable undervoltage lockout threshold (UVLO), and load current monitoring features. 

    Best Regards, 

    Elizabeth