For three level boost converter do we need just two LM5170-Q1 controller or full two EVM boards?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For three level boost converter do we need just two LM5170-Q1 controller or full two EVM boards?
Hi Muhammad,
Thanks for using the e2e forum.
According to the users guide of the LM5170EVM, it is possible to use several EVMs in parallel to increase the number of phases.
It is not possible, to solder multiple ICs onto one evaluation board.
The Users Guide for the EVM can be found on the product page:
https://www.ti.com/tool/LM5170EVM-BIDIR
If you need more details, it would be helpful to give us more information on your project, including power topology, number of phases, input/output voltage and current ranges, etc.
Best regards,
Niklas
Hi Muhammad,
I hope you made progress with your design and measurements.
As there has been no further comments, I will close this thread for now.
If you have additional questions, please reply below to re-open the thread.
Otherwise feel free to click the resolved button.
Thank you and best regards,
Niklas