Hello,
Our customer plans to use 33k-ohm+/-5% (31.35k to 34.65k-ohm) to GND on MODE pin in order to FCCM/800kHz operation. Then, he is afraid that the device does not function if the register raises higher than 30.1k+10% (33.11k-ohm) specified in the datasheet Table.-7.1.
Could you please help him out following points
- What is happened in above case.
- Does TPS548A28 works normally (FCCM/800kHz) as long as the register is set in 30.1k-ohm +/-10% range, even if +/-5% accuracy register to use.
- If possible, could you please share the MODE Selection functional block diagram with him.
Best regards,