This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ21701: Headroom needed for a 6V output

Part Number: LMZ21701
Other Parts Discussed in Thread: TPS82150

Hey team,

I have a customer evaluating the LMZ21701 for their application and they are trying to use this module in the following use-case:

Input voltage: 7V

Output range needing to support: 0.9V - 6V

Output current needing to support: Up to 1A

Will a 7V input voltage be sufficient enough to drive a 1A load at 6V? What amount of headroom is needed to support a certain output voltage? 

Best regards,

Matt Calvo