Hi,
Can you clarify what is meant by "If the sense voltage (Vs') does not have hysteresis in it, and the voltage on the sensing line contains ripples, the resetting of TL7700 is unstable" in the datasheet?
Does this mean the device might malfunction operate erratically or does it mean that the device will operate as expected but that if you have next to no hysteresis that RESET pin may trigger many times as you'd expect if the Vsense voltage is crossed continuously?
I have an application where the Vsense is 10.5V for a Vcc=12V. There's minimum hysteresis set but the Vsense is already 1.5V from the 12V rail being sensed.
Many thanks